OnMouseOver style for connected buttons and texts

News in IGSS V13 - On Mouseover style

On Mouseover style

With the new Hover Effect function you can add an extra dimension to the navigation you wish to create. By adding the Hover Effect to a Button, an immediate feedback will be visible when a mouse hovers over a connected Button, indicating that it is clickable. This new functions offer 5 different styles of hover effects. 

  1. Lighten
  2. Darken
  3. Contrast
  4. Switch colors
  5. Underline text

Normal Button State 

On MouserOver Button State


To Summarize the News

With the new On Mouseover style you get:

  • All new predefined and dynamic (now operator) graphs.
  • Complete re-write of IGSS graphing module.