New Embedded Trends

News in IGSS V13 - Embedded Trends

New Embedded Graphs

Embedded graphs are displayed as an integrated part of the process diagram in which they are embedded. In addition to that, the embedded graph displays real-time data as a function of time.

The Embedded graph user interface has also been updated and is up-to-date with our operator graph. The functionalities available in the embedded graph are the same as those found in the operator graph, in order to maintain consistency. The embedded graph is fully customizable and can be customized as you wish.

Analog and Digital Signals

Compare Periods

To further analyse your processes, you can compare one periode against another by using two time axes. The Operator can move around by dragging the axes or by using a Go to Date method. 

 

To Summarize the News

With the new Embedded Trends you get:

  • All new predefined and dynamic (Embedded) graphs.
  • Complete re-write of IGSS graphing module.

  • Improved performance
      - Faster retrieval of data due to improved log file format.
      - Data is read in the background.
      - Smart use of all available historic data.

  • Mix different data sources in same graph
      - Access to month, day and hour reductions as well as base (BCL) and log.
      - “Auto” data source – smart use of both reduced and logged data.

  • Frequent operations are made easy
      - Alter period by simply scrolling back and forth.
      - Easy predefined periods like “Today”, “1 Week Back” etc.

  • More interactive
      - Most common end user actions available in toolbar.
      - Add signals to existing graphs directly from mimic.
  • Better overview
      - Full graph overview while zooming.
      - Show individual data points.
      - Multiple value axes with same value range are automatically hidden.
      - Digital axes are stacked and only showing used states.

  • Full data precision
      - No down-sampling of data.
      - No graph if data is not present.
      - Never miss another spike.

  • New possibilities
      - Show title above graph.
      - Change legend placement.
      - Up to 16 signals in one graph.
      - Multiple time axes – compare with another period.