Visibility

News in IGSS V12 - Less is more

Visibility

To design diagrams with situational awareness in mind we also made it a lot easier to show or hide descriptors pending the state of an object.

Visibility Dialog


This enables the designer to: 

  • hide special info until needed.
  • highlight something when an alarm needs attention.
  • only show some controls in situations they are meaningful.
  • create custom alarm indication.

All this keeps the diagram free of noise and irrelevant information while the system is running normally.