Notifier SMS Cloud Service

News in IGSS V12 - Modem trouble no more

Instead of using a modem. It is now possible to receive and send SMS messages using the cloud. This could be a preferred option in areas with bad mobile coverage but stable Internet.
Setting up Cloud services for SMS
Currently the online SMS services from Twilio and TextMagic are supported.

Holidays

Also new in Notifier for IGSS V12 are Holidays. Instead of manually entering Holidays. It is now possible to import a list of holidays to Notifier.
Holidays import
Holydays are shown in the Calendar and are used in the Duty Planer to define recurring duties for these specific dates.