Improved Logging

News in IGSS V12 - Optimized Data Logging

To improve data collection and performance we worked on our log system. We have:

  • Improved logging dead band options
      - Relative change or full scale.
      - Change as floating point value.
    This results in decrease amount
    of stored log data.

  • Increased number of log files per hour
      - For large systems (2000 objects and above)
        logs are distributed in 16 files per hour
        instead of 1.
    This results in improved read performance
    without significant write impact.
Set up logging in V12