IGSS Updater

News in IGSS V12- Maintaining IGSS Software On Site

The update program has been completely rewritten in order to make it easier updating all IGSS Servers and Clients. This means you can update all stations that are not on the Internet directly from one station where an update package is available as zip or by download.

IGSS Update Program

How stations are updated in V11

IGSS Update Maintenance in V11

How it's done in V12

IGSS Update Maintenance in V12

  • Offline upgrade of IGSS server software
    New versions may be validated in the office before installing on site.

  • Clients are upgraded from the IGSS server
    Upgrades are pushed from IGSS server to operator stations.
    Update status of stations in is present in the Master System Monitor tab.

  • Updates may be rolled back.