Dashboard new Widgets

News in IGSS V12 - Monitor you key values

Two new widgets to present analog object values have been added to the Dashboard. These are a Meter and a Bar where alarm limits and setpoint are shown if defined for the object.

The Meter and the Bar here on the left of the Dashboard:

Dashboard with bar and meter

As the new Widgets takes most of it properties from the object they are connected to, the only Widget specific property available is if the bar should be drawn vertically or horizontally.