Pipes and Lines

Pipes and Lines have been merged into one tool with the property settings determining whether you draw lines or pipes. This enables the System Designer to draw lines and pipes quicker and with greater control over the end result. Pipes are no longer drawn using the Animated Symbol feature in IGSS, although the feature has not been disabled in order to ensure backwards-compatibility with older versions of IGSS.

Enlarged image Line Start and End points can be defined, selecting arrow end points and bullet-type start points.