Notifier Status Objects can be used to monitor the state of the Notifier module.
Holidays can be defined for the entire Notifier module and Duty plans can be created to include or exclude defined holidays. Entire calendars can be copied and edited, decreasing the time required to manage duty plans and calendars in the Notifier module. SMS messages can be defined and sent to selected Notifier operators or all Notifier operators, informing them of important events, for example the start of their duty or changes in the duty plan.
Maintenance jobs can be copied, either by job type or by object to speed up maintenance job creation. The maintenance filter feature has been augmented and the start time for periodical maintenance jobs can be defined.
Users alarm acknowledge using the Notifier module can be logged in the Audit Trail database.