Free Value Object Atoms

Three new atoms for analog objects have been added: Free Value 1, Free Value 2 and Free Value 3. The Free Value atoms can be used to store numerical values from a PLC in LOG files only, each atom mapping to a PLC address of your choice. Free Value atom data can be displayed in graphs and reports as well as in descriptors in diagrams and may be formatted individually to display units and number of decimals. Free Value atoms cannot trigger alarms.

Free Value Atoms

Additionally, Free Value atoms are included in the calculation functions.