Diagrams and Areas

You can add diagram navigation to IGSS buttons. The enables the user to navigate backwards or forwards in the list of Most Recently Used (MRU) diagrams.
Navigation Buttons In IGSS

Further in System Configuration the Diagrams can be set to remain open when changing Area.

And now Graph, Area and Diagram descriptions can be used instead of Graph, Area and Diagram names in the Supervise menu.