Automatic Screen Resolution Scaling

Configurations created on a system with one screen resolution can be opened on systems with another screen resolution without changing the screen resolution registered in the configuration. The System Designer can select to scale the configuration with the present screen resolution or keep the screen resolution registered in the configuration.