Alarms and alarm counter

For objects with multiple digital alarms, you can view alarm details of each alarm as well as selecting which alarm to read or edit alarm notes for.

The Alarm counter parameters are increased, allowing you to specify which types of alarms are to be included in the alarm number displayed in the alarm counter.

Real-time alarms can be displayed in the Active Alarm form when using the IGSS Playback feature to display historical data in the Supervise module.