New auto save function
A new auto-save option has been added to the Notifier Options. When set the Notifier confuration file will
automatically be saved when required without any need for user interaction.
3 new operator modes
A new system setting has been added to Notifier that makes it possible to restrict the access of the system operator to
the Notifier configuration.
CalendarMode:
0 = > Advanced (Default)
- No restrictions for the system operator.
1 => Basic
- The Calendar can be edited with duties, duty personnel and filters.
2 => Novice
- The Calendar can be edited with duties, duty personnel and filters.
- Duty personnel and filters can be created, modified and deleted.
3 => Strict
2
- Duty personnel alone can be added to or removed from existing duty plans only.
New dual server mode
It is now possible to configure the Notifier module for operating in dual server configuration. On the backup server,
Notifier may be configured to monitor the Notifier module on the primary server. As long as the primary Notifier is
running, the Notifier module on the secondary server will not transmit any alarms. If the backup Notifier is not able to
connect to the primary server, it will become active and start transmitting new alarms.
Coloring of exception days in the calendar
If an exception is added to a recurring duty in the Notifier duty plan, the day of the exception is marked with a special
color. This indicates to the operator, that this date will be handled special.
Trigger alarm in IGSS if GSM modem does not reply
If, for some reason, the Notifier module is unable to communicate with the attached GSM modem, it is possible to
raise an alarm in IGSS by setting the value of a digital object in IGSS.