Embedded Alarm List Directly on Diagrams

To improve the overview for the operators, IGSS supports embedding of alarm lists directly on the diagrams. This will make it possible for the user to configure overview diagrams for plant sections containing their “own” alarm lists and in a more general way making it possible for each diagram to present its “own” alarms.

Technically, the alarm list will show alarms matching a specific filter. It will be possible to configure which columns to show and whether or not it should be possible to acknowledge alarms from the diagram.