An alternative to the dualized server is the Single User Server Backup station. In this case, only one genuine server is installed. The IGSS operator station designated as Single User Server Backup runs as a normal operator station as long as it can maintain a connection to the IGSS server. If the connection fails, either due to network error or IGSS server error, the operator station will restart in the Single User Server Backup mode and assume the role of the IGSS server.
When the connection to the IGSS Server is re-established, the data collected while the station was running in Single User Server Backup mode can be synchronized with the server.
Please be aware that the server can only synchronize data from one Single User Server Backup station.
Single server