To provide optimal flexibility and overview, the IGSS package supports up to 9 monitors for any given IGSS system or configuration. Control room personnel are thus provided with a user-friendly overview of the process whose various diagrams would typically be allocated to different monitors for creating a more logical and better organised view of the plant.
Monitors can be either stacked or placed adjacently to one another, or a combination of the two. For each monitor used, a separate graphic card must be installed on the IGSS server.
Horizontal and vertical monitor setup