Allen Bradley SLC5 Series TCP/IP driver ID:87
Interface Description
There is presently no additional information regarding this driver available.
If you require information regarding the specifics of this driver, please contact IGSS Support.
Technical Data
Electrical Interface | : | - |
Protocol | : | - |
Types of data | : | - |
PLC types supported | : | - |
Addressing | : | - |
Supported platforms | : | - |
Max. telegram size | : | - |
Transmission speed | : | - |
Communication mode | : | - |
Throughput | : | - |
Max. number of channels | : | - |
Max. number of nodes | : | - |
PC hardware requirements | : | - |
PC software requirements | : | - |