• Russian

Data file interface driver ID:50


Interface Description

IGSS32 offers a driver for periodically reading of a specified CSV file. The file contains information on data type, address and date/Time. The driver may delete the file after read and wait for a new to be created by 3.rd party.

Technical Data

Types of data:Word=0, Dword=1 and Float=2.
Addressing:Type, Offset, Value. ex. 2, 9, 00870
Supported platforms:Windows Vista, Windows XP, Windows 2003 Server, Windows 2000
Max. number of channels:Up to 8 Nodes (csv files) is supported.
PC hardware requirements:None.
PC software requirements:None.