Mitsubishi Q/FX Series (TCP/IP) ID:89


Interface Description

There is presently no additional information regarding this driver available.

If you require information regarding the specifics of this driver, please contact IGSS Support.

Technical Data

Electrical Interface:-
Protocol:-
Types of data:-
PLC types supported:-
Addressing:-
Supported platforms:-
Max. telegram size:-
Transmission speed:-
Communication mode:-
Throughput:-
Max. number of channels:-
Max. number of nodes:-
PC hardware requirements:-
PC software requirements:-