FLYGT AquaCom ID:69


Interface Description



Technical Data

Electrical Interface:Rs232C
Protocol:AQUACOM protocol
PLC types supported:FMC-200
Supported platforms:Windows Vista, Windows XP, Windows 2003 Server, Windows 2000
Transmission speed:Up to 115Kbaud depending on the PLC port speed.
Max. number of channels:8 channels
Max. number of nodes:255 nodes.
PC hardware requirements:1 to 8 standard serial ports (COM ports). Standard modem(s) if dialled-up is used