Phoenix Fernwirk protocol driver ID:62


Interface Description

IGSS32 offers an interface for Phoenix WT45 equipment using Fernwirk Protokoll. Fernwirk Protokoll is a master slave protocol that can be used in both point-to-point and in multidrop configurations. The IGSS32 driver implements direct point-to-point, dialled-up and radio connections to Phoenix WT45 equipment equipment. The communication interface is also capable of reading historical sampled data in Phoenix WT45 stations, thus making it possible to make reports and show graphs of signals stored in the Phoenix WT45 eventhough it is not directly connected all the time (e.g. in dialled-up configurations). The IGSS32 system polls the PLC equipment cyclically according to one of four user-defined time intervals. The time intervals are configurable from 100 milliseconds to 999 seconds. The system automatically groups process data in data blocks - thus fully exploiting the the communication link in relation to the present configuration.

Technical Data

Electrical Interface:RS232C.
Protocol:Phoenix ReSY Protokoll
Types of data:Bits, Bytes, Words and Dwords
PLC types supported:WT 4500, ILC 200 IB, ILC 200 UNI, ILC 350 ETH, RFC 430, RFC 450, FC 200 PCI, FC 350 PCI
Addressing:Node (PLC), block (DB), word (16 bit), bit offset.
Supported platforms:Windows Vista, Windows XP, Windows 2003 Server, Windows 2000
Max. telegram size:56 bytes
Transmission speed:19200 baud
Communication mode:Half duplex
Throughput:Contact Developer Flemming Petersen at
Max. number of channels:Up to 8 COM Ports are supported.
Max. number of nodes:255
PC hardware requirements:1-8 standart seriel ports (COM ports). Standard modem(s) if dialup is used.
PC software requirements:None