SQUARE-D Multidrop COM port protocol driver ID:60


Interface Description

IGSS32 offers an interface for the Square-D PLC equipment. The Square-D interface is designed to connect the IGSS32 system with one or more Square-D PLCs via the PC COM ports with a RS-232C TO RS-422 converter.

Point to Point connection are supported through a RS-232c/RS-422 converter directly to the CPU port on the PLC. It is also possible to address more PLCs on the SY/LINK network. Using the SY/LINK network requires the connected PLCs to be equipped with a network itnerface board.



The IGSS32 system polls the PLC equipment cyclically according to one of four user-defined time intervals. The time intervals are configurable from 100 milliseconds to 999 seconds. The system automatically groups process data in data blocks - thus fully exploiting the the communication link in relation to the present configuration.

Technical Data

Electrical Interface:RS-232C.
Protocol:SY/MAX FAMILY COMMUNICATION PROTOCOL.
Types of data:String, Fixed Point 8, 16, 32, BCD 16, 32, Float 32, Timer, Counter.
PLC types supported:All Square-D systems supporting SY/MAX or RS-422 connections.
Addressing:Node (PLC), Data register number, bit offset.
Supported platforms:Windows Vista, Windows XP, Windows 2003 Server, Windows 2000
Max. telegram size:256 byter per Telegram.
Transmission speed:9600 baud.
Communication mode:Half duplex.
Max. number of channels:1-8 channels (COM ports) are currently supported.
Max. number of nodes:up to 255 nodes per channel, max 1024 nodes
PC hardware requirements:1 to 8 standard seriel RS-232c ports.
PC software requirements:None