Omron FinsGateway Driver ID:52


Interface Description

The IGSS32 Omron FinsGateway communication interface offers connection to all Omron PLCs supported by the FinsGateway communication package. The driver supports a number of different network types including Serial RS232, Ethernet, Sysmac Link and Controller Link.

For more information on Omron FinsGateway, supported networks and PLC types please look at:
http://www.plcsoft.ne.jp/soft/Eng/Info/FinsGateway/

The driver requires Omron FinsGateway to be installed.

Technical Data

Protocol:Fins
Types of data:DM and CIO Memory
PLC types supported:All Omron PLCs supported by Omron FinsGateway
Addressing:Word and Bits
Supported platforms:Windows Vista, Windows XP, Windows 2003 Server, Windows 2000
Max. telegram size:Network dependend
Transmission speed:Network dependend
Communication mode:Polling and event driven communication
Max. number of channels:Up to 4 concurrent communication units supported
Max. number of nodes:Up to 256 concurrent nodes
PC hardware requirements:Applicable network interface board or serial ports
PC software requirements:Omron FinsGateway version 2 or higher