Omron SysMac Link Driver ID:49


Interface Description

The IGSS32 Omron SysMac Link communication interface offers connection to all Omron PLCs equipped with a SysMac Link interface. The driver uses a dual port RAM interface on the PC to communicate with an Omron SysMac Link PC interface board. No other PC driver SW is required.

Technical Data

Protocol:Omron Proprietary
Types of data:All applicable types of data
PLC types supported:All Omron PLCs equipped with a SysMac Link interface
Supported platforms:Windows Vista, Windows XP, Windows 2003 Server, Windows 2000
Max. telegram size:256 Words
Transmission speed:1 MBits/s
Throughput:Up to 8 telegrams pr. second
Max. number of nodes:63
PC hardware requirements:Omron Sysmac Link interface board
PC software requirements:None