Gascromatograph file interface driver ID:47


Interface Description

IGSS32 offers a driver for periodically reading of a specified CSV file. The file contains information on data type, address and date/Time. The driver will delete the file after read and wait for a new to be created by 3.rd party.

Technical Data

Types of data:Float.
Addressing:Address, Name, Date, Time, Value. f.ex: 7, Propane, 14-SEP-2001 13:32:59.55487, 0.0856.
Supported platforms:Windows Vista, Windows XP, Windows 2003 Server, Windows 2000
Max. number of channels:One channel (file) supported.