B&K 1301 IEEE 488 Interface Driver ID:35


Interface Description

The driver uses a GPIB IEEE 488 interface board to communicate with a B&K 1301 spectrometer.

Technical Data

Electrical Interface:GPIB IEEE 488
Protocol:GPIB IEEE 488
PLC types supported:B&K1301
Supported platforms:Windows Vista, Windows XP, Windows 2003 Server, Windows 2000
PC hardware requirements:GPIB Interface board
PC software requirements:GPIB protocol software