Sabroe&Soeby COMSAB II ID:23


Interface Description

IGSS32 offers an interface for connecting to COMSAB II gateways. COMSAB II gives the user access to read and write data in the following SABROE compressor control units: PROSAB II, UNISAB S/R/RT/RTH and UNISAB II. The COMSAB II functions as a gateway, converting from the proprietary HDLC/RS485 protocol, which is used between the compressor control units, to a simple ASCII/RS232 protocol.

The IGSS32 system polls the compressor control units cyclically according to one of four user-defined time intervals. The time intervals are configurable from 100 milliseconds to 999 seconds. The system automatically groups process data in data blocks - thus fully exploiting the the communication link in relation to the present configuration.

Technical Data

Electrical Interface:RS-232C.
Protocol:SABROE 0178-400 protocol
Types of data:Most available data points in the compressor control units are available for reading and writing.
PLC types supported:SABROE compressor control units: PROSAB II, UNISAB S/R/RT/RTH and UNISAB II.
Supported platforms:Windows Vista, Windows XP, Windows 2003 Server, Windows 2000
Max. number of nodes:14 pr. COMSAB II unit.
PC hardware requirements:Standard serial RS-232C port.
PC software requirements:None